This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914Q-Q1: Question of FPD link level

Part Number: DS90UB914Q-Q1

Hi team,

 

Can you please review an issue of FPD-Link level in DS90UB914Q?

 

In the swapping test of PCBs and camera sensors, the failure depends on PCB#1.

 

PCB#1 : Impedance=96.5ohm, FPD Link level= below 500mV -> Video data is unstable

PCB#2 : Impedance=99.5ohm, FPD Link level= 740~800mV -> No issue

PCB#3 : Impedance=99.5ohm, FPD Link level= 740~800mV -> No issue

 

Question.

1. What is the tolerance range for 100ohm impedance? Is it acceptable for +/-10ohm variation in PCB?

2. For the level of < 500mV on DS90UB914Q, what is the expected problem? Is there any way to adjust the level? 

Thanks,

Sam Lee