This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I: About VDD and VDD33 supply ramp requirements

Part Number: TUSB4041I

Hello support team,

I have a question about TUSB4041I.

Specifications of "VDD33 supply ramp requirements" and "VDD supply ramp requirements" are described in section 7.6 "Power-Up Timing Requirements" in the datasheet.
Both specs are 0.2 ms to 100 ms.

If rise time or fall time of VDDs deviate from these specifications, what kind of problem will happen?
For example, what side effects can be considered if the rise time of VDD33 is earlier than 0.2 ms?

Sincerely,
M. Tachibana