Part Number: DS100BR111
Other Parts Discussed in Thread: DS125BR111, SN75LVCP600
Dear,
I made an electronic design for embedded computer needs, that integrates SATA III link for which I add DS100BR111 repeaters. The SATA links are issued from Intel 6th generation Core i5/i7 processor on COM Express type 6 module.
I found the best pin configuration for the two repeaters I use, but the operation of the link is very unstable. It looks like the repeater causes a dysfonctionnement of the autonegociation of SATA link because sometimes when it well boot on the OS, the both SSD used are in 6Gb/s with good performances, but more often they are not in full speed or viewed in BIOS but not in Windows7 and 10...
Bypassing the repeater permit a best autonegociation process and the disk are always viewed in BIOS and OS, but performances are under.
Is there any "normal" explanation of this problem and any way to correct it?
Thanks for your help.
Romain