Part Number: DS80PCI810
Other Parts Discussed in Thread: TIDA-00423
Hi
I have a desire to use the DSP80PCI810 in a hotswap 85ohm PCIe Gen3 application.
Has there been any testing with the DSP80PCI810 in an 85 ohm environment? Differential traces are 85 ohms, Root complex and endpoints terminated at 85 ohms.
There's a sentence in the datasheet that states: "If 50 ohm impedances are seen on both positive and negative output of a DSP80PCI810 channel, Rx detect state machine asserts Rx detection". So, what happens if 42.5 ohm +/-10% impedance is seen? Will the Rx detect state machine still assert RX detection?
Thanks,
Jason