Part Number: DP83TC811R-Q1
I'm trying to design the 100BaseT1 PHY into our system and ran into the following strapping questions (and a few other questions):
- Is there an internal Power On Reset function? The datasheet seems to imply that there is, but it’s not explicitly stated. In other words, does it need a reset signal input, or will it POR on its own if the reset pin is left floating?
- One cannot use the default strapping of RX_D0 - RX_D2 because that would be MAC[2:0] = 0, which is Reserved per Table 20. Correct? This seems odd that the default configuration is not a valid one.
- On strapping the LED_0/1, Figure 28 shows the connection, but Rp is not specified. What resistor value should be used?
- On strapping the LED_0/1, what’s the default if no strap is applied (i.e. only the LED and current limit R)? Figure 28 shows no default, yet Table 18 lists a default.
- Is there an errata for this PHY?
Thanks for any info on these items.