Part Number: SN65HVS885
If there is a voltage of 24 volts on one input(like IP0) and a ground on another(like IP1 or the rest of the pins), would these pins be able to handle this kind of function if the ground for the chip is accidentally disconnected from the input cable(basically becoming a different GND)? Would there be any adverse effects?
Regards,
Ramon