Part Number: SN65DSI84
Hi Sirs,
Sorry to bother you, we have some question on SN65DSI84
- The SOC isNXP iMX8M, display signal is MIPI-DSI (1-4 lanes, 1920x1080, 60Hz, use SN65DSI84 to transfer dual LVDS. There have two LVDS panel, one is 1024x768 (10.4”) and another is 1366x768(10.1”),so do we only need use SN65DSI84 single-link? or need use dual-link?
- SN65DSI84 spec Suitable for 60-fps WUXGA 1920 × 1200, Resolution at 18-bpp and 24-bpp Color, 60 fps 1366 × 768 at 18 bpp and 24 bpp, is mean could support single-link and dual-link the max resolution spec?
- If we need use dual LDVS panel, just choose dual-link? if yes, how about the LVDS max resolution supported?
Thanks for your reply