Part Number: DS92LV18
Hi,
I am working on a design with full duplex LVDS Ser/Des using DS92LV18. (Let's call Side 1 and Side 2 the two LVDS side in point to point bidir full duplex operation)
Side 1 has a FPGA that manage clocks TCLK and REFCLK.
Side 2 only has an oscillator generating REFCLK (5% max of TCLK). For the TCLK of side 2, I wonder if it's better to use either autogenerated clock : RCLK ou to also use the oscilator that generate REFCLK.
What would be the best practice according to you ?
Best regards
Adrien