Part Number: TCA9617B
Other Parts Discussed in Thread: TCA9517A
I have a design where in my I2C master is at 3.3V and I2C slave is it 2.5V, I am looking for a suitable Level translator.
When i looked at a few Repeaters/Translators' i see most of the application examples shown in the datasheet are of the type "master is at Lower voltage side" and "Slave is at higher voltage side",--does this mean i can't use these kind of devices in my application?
For Example in TCA9617B device,
Can i connect the master to VCCA side at 3.3V and Slave to VCCB side at 2.5V?
OR
Can i connect master to VCCB side at 3.3V and Slave to VCCA side at 2.5V?
OR
Suggest me a suitable translator for my application.