Hello,
Regarding the following statement from an earlier post, titled DS26LV32AT from May, 2012:
"The RS-422 inputs are specified to take +10V to -10V input levels and adhere to the RS-422 input current specification. These inputs are very robust, I do not expect them to be the problem."
Are the RS-422 inputs able to tolerate active signals when the IC is powered down, i.e. 0 V on Vcc?
Thank you,
Leo