Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: DP83867IS function setting question

Part Number: DP83867IS
Other Parts Discussed in Thread: DP83867E

Hi, 

Our customer has some questions need confirm as below:

1) RX_CTRL mode setting definition(See DP83867IS DS page 37)

    For Autoneg Disable function, if customer wants setting Autoneg enable will setting "0"(MODE3), right?

2)The clock pin relative of GPIO_0,GPIO_1,LED_2,LED_1 mode setting definition(See DP83867IS DS page 37)

   Normally, should be setting MODE"1", right?  If yes, when will setting table 8 and table 9?  (See DP83867IS DS page 38/39)

3)For LED_0 setting(See DP83867IS DS page 38)

   If customer wants Mirror Enable setting "1", and wants SGMII Enable setting "1" =>Mode4

   Else if customer wants Mirror Disable setting "0", and wants RGMII Enable setting "0" =>Mode0, correct?

4)For Mirror definition, we can see "DP83867E SGMII EVM User guide" page 12.

   For J18 to T1 connection, T1 double A connect to J18 pin 7/8.

                                             T1 double B connect to J18 pin 5/6.

                                             T1 double C connect to J18 pin 3/4.

                                             T1 double D connect to J18 pin 1/2.

 And base on  DP83867IS DS page 35 Mirror mode definition: A->D,B->C need set mirror mode to enable(1), right?

Warm Regards,

Kevin Lin