This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9617B: connect A side and B side in one star topology

Part Number: TCA9617B

Hi Team,

As below diagram, when TCA9617 used in star topology, can connect A side with B side together with Master?  could it be problem?  thank you.  

  • Hi Lilian,

    Yes, the circuit that you showed would be OK. The case you want to avoid is having multiple B sides connected on the same node, since the "low" level output from one B side would be too high to be detected by the other B sides (this is important in how the device handles bidirectional communication). In this diagram, though, it looks like there is only one B side connected to multiple A sides, so you will not see this problem.

    Regards,
    Max