Part Number: SN75LBC175
Hi,
We have been using the SN75LBC175AD chip before.
Description:
1. The last 60 ICs were purchased, but there are two batches: 51ADFFM and 5BA2GKM.
2. The problem that we are now facing is that we have unrecognized problems after we access the AES signal. The technical indicators we measure are unqualified.
3. The datasheet shows that the threshold voltage is 0.2V to identify the signal, but this batch of chips is very unstable, some are in 1V, and some even reach 3V.
4. The previously used chip can guarantee that our board AES minimum input voltage is 0.16-0.2V; this time the minimum input voltage of the purchase chip is 0.3V-3V.
The threshold voltage of 75LBC175A is less than 0.2V, and the chip we purchased this time cannot reach 0.2V (even 3V phenomenon). It means that there is a problem with the chip. In addition, there are 2 batch numbers in the board.
5. But the problem disappears when we replace the previously purchased chip with the PCB board of the newly purchased chip.
6. Is there a problem with our use, or is there a problem with this batch of products. Or we did not notice those problems during use.
7. How to detect the quality of this chip?
Thank your for your help.
Regards,
Eric