Part Number: TPS25810
Other Parts Discussed in Thread: HD3SS3212,
Team,
TPS25810+HD3SS3212 solution is recommended in TPS25810 datasheet. Is there any method that we can omit the SS MUX?
Regards,
Nic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
.If the system can allocate two ports to support the both orientations on a USB-C port, there is no need for the mux.
Windows 10 should support Type-C ports that do not use a MUX for the two orientations of the SS lines, but instead allocate two ports(one for each orientation). The ports should be as described in ACPI, refer to the section 9.14 of the latest ACPI specification.
ACPI spec can be downloaded from here: