This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6501: SN6501 application recommendation

Part Number: SN6501

Could we use SN6501 + LDO to design a 5Vin / 5Vo Io = 300mA power supply? 

could you help recommended the transformer and LDO part number?

Thanks.

  • Hi Robin,

    Thank you for posting your question on the E2E forum.

    1) For the desired specs,  especially the 300mA load, the SN6501 will be too tight, since it's max current capability @ 5V is only 350mA.  Since we need to use a step-up transformer to account for drops across diodes and the LDO,  we need more margin in the spec.  For this reason, I'd recommend the SN6505 solution. It can provide up to 1A and therefore is an excellent solution.

    2) For the transformer, do you know if you need basic isolation or reinforced isolation? For Basic Isolation (2.5-kVrms)  you can use the following transformer from Wuerth : 750315371 and for reinforced (5 Kvrms)  you can refer to 750315240, also by the same  company. These are for examples only. You/your customer can pick a similar spec transformer from their preferred vendor.

    3) For the LDO, you can use a TI TPS76350 or TPS76701QD, or some other TI LDO with similar specs.

    For convenience, the SN6505 EVM  and User Guide for the above solution (including schematics and full BOM) is available here

    Table 3 in the SN6505 Datasheet is also a good source for transformer part numbers (Page 24).

    Hope this helps!

    Regards,

    abhi

  • Hi Abhi,

    Thanks very much for your kindly help!

    Regards
    Robin Liu