Part Number: HD3SS215
Hi!
I built up a prototype to switch between two HDMI sources and output to a display. It seems to work fine with sources that are initially HDMI outputs (from laptop or Chromecast). When I try to connect a source that's originally DP (using a DP to HDMI cable from a PC laptop), or USB C (Macbook Pro USB C to HDMI converter, then HDMI cable), the output is either black or very unstable. The source device registers that there's a second display connected. From the datasheet, it doesn't seem like the HD3SS215 chipset would differentiate between these since the signals have been converted to HDMI, but is there something more to it? The sources work on the display individually.
Thank you!