Part Number: SN65LVDT41
Other Parts Discussed in Thread: SN65LVDT14, DRV8860
Regarding the VIH levels for the D or R inputs of the SN65LVDT14 and SN65LVDT41, can I assume that these inputs can safely tolerate 5.7V? The reason I ask is that I plan to drive these inputs with the Dout of a DRV8860 (also a TI device) and this Dout is internally pulled to 5.7V in the DRV8860. The absolute maximum is 6V but there is no maximum voltage for VIH in the Recommended Operating Conditions.
Regards,
James