Part Number: TCA9539
Other Parts Discussed in Thread: TCA9535,
The DS of the TCA9535 says:
"the TCA9535 does not include the internal I/O pull-up resistor, which requires pull-ups and pulldowns on unused I/O pins when configured as an input and undriven."
I cannot find such information in the TCA9539 DS. Does this mean I can leaf unused input pins floating on the TCA9539?
I have an application where it is neccessary to switch pins to high-Z (by configuring them as inputs) without having a pull-up or pull-down connected.
If I have to pull the inputs to a defined state, what is the max. possible resistor value I can use?
Thank you!