Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2046I: Connection with TPS2552

Part Number: TUSB2046I
Other Parts Discussed in Thread: TPS2552

Hello.
TUSB2046I is driven by 3.35V.
TPS2552 is driven by 5V.

Is the connection of these devices correct in the figure below?

TUSB2046I-TPS2552.pdf

The OVRCUR-input is pulled-up by 3.3V because the FAULT-output of TPS2552 is open-drain.

The PWRON-output is not pulled-up because the PWRON-output is push-pull.
The conditions of the EN-input of the TPS2552 are described below


Page-6
"7.3 Recommended Operating Conditions"
 VEN  Enable voltage    0V to 6.5V
 VIH  High-level input voltage on EN   MIN 1.1V
 VIL  Low-level input voltage on EN   MAX 0.66V

Regards,
Dice-K