Part Number: TUSB4020BI
Hi
I would like to know how PWRCTL_POL and PWRCTL1/2 behaves when the USB is pluged in.
On the datasheet, PWRCTL_POL and PWRCTL1/2 is sampled after reset. However I do not understand how it behaves at each pin.
If PWRCTL_POL = Pull down = Low, the polarity is "active high" and PWRCTL1/2 will be set to low. Is this correct?
Then , PWRCTL1/2 will be high whent USB is pluged in. Is this correct?
(This is our measurement result on the customer board actually.)
Does PWRCTL1/2 set to High (PWRCTL_POL=0) or Low (PWRCTL_POL=1) internally when USB is plugged in?
(I could not find on the datasheet about the those pin behaviors when USB is plugged in.)
Best Regards,
Koji Hamamoto