Part Number: DS90UB913A-Q1
[ DS90UB913A-Q1 ] 10-bit 12-bit Mode Switch with Register
Hi,
Can you help to clarify whether 10-bit/12-bit mode can be switched with DS90UB913A-Q1's 0x05 register?
From the datasheet, it seems that these registers are read-only, however, other thread (see related link) discussed that 10-bit or 12-bit can be switched by changing these read-only register.
Can you confirm whether 10-bit and 12-bit mode can be switched with these registers?
Also, the related post indicates that bis map is also not valid. Can you check this as well?
Thanks,
Ken