Part Number: DS90LT012AQ-Q1
Hi
We refer AN-1194 application report.
http://www.ti.com/lit/an/snla051b/snla051b.pdf
In this user guide, there is the example figure of external failsafe as Figure 3.
IN+ : R1=8K pull up
IN- : R3 = 4.99K pull down
These resistor value would offer output HIGH when open input failsafe occurs.
If output LOW is required, could it be correct to swap R1 and R3?
BestRegards