Part Number: TUSB8041
Other Parts Discussed in Thread: AM5706
Hi Team,
My customer is using TUSB8041 to connect to AM5706, the potential volume is big. In fact, customer just need USB2.0, but we only have USB3.0 and USB1.1, so we penetrate TUSB8041. Can you help double check the schematic, thanks for the support!
At the same time, two important question need douoble confirm:
1. Pls also help double confirm R1109,C819,R1111 value? It seems some difference between datasheet and our reference schematic. Need expert help confirm it as well.
2. For each port, customer don't use the 5V VBUS, is this ok(If slave already powered itself)?
Best regards,
Sulyn