Part Number: DS90UB927Q-Q1
Hello,
VDDIO input, what is the difference between 3.3V and 1.8V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VDDIO could be 3.3V or 1.8V. This depends on the Interfacing part to 927.
Hi, Vickers
Please understand it from the other viewpoint.
UB927 can support both 1.8V and 3.3V I/O voltage, can be flexible to link with other device without the need of the level shifter, this is UB927's benefit. for example, If the paired part (in general it is processor...) with UB927 only can support 1.8V I/O voltage, you should provide UB927 the 1.8V VDDIO.
best regards,
Steven