Part Number: TCA9406
Other Parts Discussed in Thread: TCA9517A, TAS5766M, , TCA9517, PCA9306
Hi,
I posted following question to audio amplifier forum.
A customer wants to connect TAS5766M with 5 volts I2C-bus he used to use. But TAS5766M is not able to connect with 5 volts I2C-bus directly, because SCL and SDA are not 5 volts tolerant terminals. Therefore he thought to put Level-Shifting I2C Bus Repeater such as TCA9517A between TAS5766M and 5 volts I2C bus. But VOL of TAS5766M does not satisfy VILC of TCA9517A. Is there any good solution?
The answer of audio amplifier forum was...
'We used the TCA9406 in one of our audio EVMs. You can take a look at this device.'
The maximum VOL of 3.3 volts I2C slave device TAS5766M is 0.22 x VDD (= 0.762 V). Can we use TCA9406 in this case?
Best regards,
Akio Ito