Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75LVCP601: Use as USB3.0 Redriver

Part Number: SN75LVCP601
Other Parts Discussed in Thread: TUSB522P

Hi Team,

Is there any objection or pitfalls in using the SN75LVCP601 as an alternative to the TUSB522P to redrive USB3.0 signals? Reason I ask is that customer is already using the SN75LVCP601 for it's intended purpose and would like to try and make it work for USB too.

Looking over the two datasheets, both appear to be super similar even though they comply to two different standards. What makes me think this might work is that the OOB threshold on the SN75LVCP601 is 150mVpp and the LFPS threshold on the TUSB522 ranges from 100mV to 300mV. Seems to be in the same ballpark. Could it work?

Any clarity of help you can provide would be awesome!

Thanks,
Mitchell