Part Number: DS90UB954-Q1EVM
Hi,
We have DS90UB953/954-Q1 EVM and I downloaded the "Analog LaunchPAD" and "954_953_sensor_setup.txt" file.
Communication is normal, but the following error is displayed when I run the script.
>*** Running 954_953_sensor_setup.py ***
Sensor Reset
Traceback (most recent call last):
File "<input>", line 1, in ?
File "C:\Program Files (x86)\Texas Instruments\Analog LaunchPAD v1.57.0010\954_953_sensor_setup.py", line 41, in ?
NameError: name 'regAddr' is not defined
*** Script execution time 0 min 1.263 sec ***
>
What is wrong in order to increase the data transfer rate?
If "ovt_1280_1080_30fps_REMOTE.py" is needed, please send me it.
Best Regards,