Part Number: DS90UB934-Q1
Other Parts Discussed in Thread: TMS320DM365, DS90UB954-Q1
Good day,
I have an application with DS90UB934 connected to two cameras with DS90UB933 serializers on RIN0 and RIN1. We would like to multiplex both cameras to get a 12fps min rate at HD resolution (1080x1920) for each camera.
We find however that when switching between inputs it takes too long fro re-sync ("lock") and we are only capable of approx 2.5fps. Is there a way to speed up the "lock" speed when switching between cameras?
I notice there is a mention of Frame sync using GPIO but no further app note or explanation of this anywhere?
Any help or pointing in the right direction will be greatly appreciated.
ps. I had a look at the DS90UB954 but we are interfacing to TMS320DM365/8 device without MIPI CSI-2 interface so it becomes too complicated.