Part Number: TCA9406
Other Parts Discussed in Thread: TCA9617B
Team,
I have a customer presently using TCA9406. There is a section in the datasheet that I would like some clarifications on, copied below. What concretely speaking are the system design constraints? Regarding signal trace lengths can I infer that 15ft in free space and 7.5ft in FR4 are the conductor length limits to avoid reflections? How do I calculate the maximum capacitance?
8.3.3 Output Load Considerations
TI recommends careful PCB layout practices with short PCB trace lengths to avoid excessive capacitive loading and to ensure that proper O.S. triggering takes place. PCB signal trace-lengths should be kept short enough such that the round trip delay of any reflection is less than the one-shot duration. This improves signal integrity by ensuring that any reflection sees a low impedance at the driver. The O.S. circuits have been designed to stay on for approximately 30 ns. The maximum capacitance of the lumped load that can be driven also depends directly on the one-shot duration. With very heavy capacitive loads, the one-shot can time-out before the signal is driven fully to the positive rail. The O.S. duration has been set to best optimize trade-offs between dynamic ICC, load driving capability, and maximum bit-rate considerations. Both PCB trace length and connectors add to the capacitance that the TCA9406 output sees, so it is recommended that this lumped-load capacitance be considered to avoid O.S. re-triggering, bus contention, output signal oscillations, or other adverse system-level affects.