Part Number: ISO1540
We noticed that when bias supply VCC2 is not present (0V), the I2C lines (SCL, SDA) output appear to be in LOW impedance as opposed to HIGH impedance as stated in Table 2. Could you please check and confirm? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1540
We noticed that when bias supply VCC2 is not present (0V), the I2C lines (SCL, SDA) output appear to be in LOW impedance as opposed to HIGH impedance as stated in Table 2. Could you please check and confirm? Thanks!
Hi Koteshwar,
Though I don't have all detail measurements and tests, I was told that there a few other I2C devices were on the same bus and when the bias supply 3.3V was not present at VDD2 pin, the I2C's of all other devices were pulled down (lost communication).
The I2C bus is pulled up at 3.3V @ 2K Ohms. This is a separate 3.3V from the 3.3V at VDD2 pin.
should we simply disconnect all other devices on the bus and measure impedance between VDD2 and GND2 with a multi meter? if so, what impedance should it be?
Likewise, is it the same for VDD1?
Thanks,
Tim