Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65987D, TPS65982
Hi Team,
Are there any IRQ event or internal event to get PDO change timing in TPS65983B?
My customer want to use it for discharging Vbus line.
Regards,
Takashi Onawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Onawa-san,
The TPS65983B is only to be used for TBT3 devices following an intel reference design. May I know which reference design they are following?
Also, the TPS65983B integrates the VBUS discharge so there is no need for the customer to implement this externally.
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric
Hi Onawa-san,
The VBUS discharge circuit will also work when the cable is unplugged and VBUS must return to 0V. Typically, if multiple source PDOs are on the same power path, the DC/DC supply is responsible for discharging the source voltage to the appropriate level.
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric