Part Number: HD3SS3220
In the data sheet it states :-
Note: HD3SS3220 Does Not Care
About Differential Pair Polarity
Thus if I swap \ cross the TX1p with the TX1n signals like shown in Figure 12, does the Rx1p and Rx1n signals have to be swapped \ crossed as shown OR is there no correlation between the swapping of the individual pairs and if I need to I can swapped only the Tx and leave the Rx with the "correct" polarity ?