Hello Sir or Madam.
I'm using the TCA641E as an I2C slave in one of my designs.
There are 2 things I need to know about the GPIO pins for the TCA641E:
- Before power is applied to the GPIO chip, what is the state of the GPIO pins?
- After power is applied, but before any programming or communication has happened, what is the state of the GPIO pins?
According to the datasheet (page 7), the answer to #2 is "At power on, the GPIOs are configured as inputs with internal 50-kΩ pulldown resistors enabled; however, the system master can enable the GPIOs to function as inputs or outputs."
I could not find an answer to #1 on the datasheet, and technical support over the phone did not have an answer to #1.
I need a confirmation to both questions please, as it determines how I setup my schematic (include pullups, pulldowns, nothing at all, etc).
Thank you for your time.
Best Regards,
Jake Sheroff