Part Number: SN65LVDT101
Dears,
Our customer have some questions about SN65LVDT101. In his application, SN65LVDT101 is connected to MC100EP195 (On Semiconductor), which is a 3.3V ECL programmable delay chip. The schematic is as follows:
The 1.3V is supplied by a LDO, the max current the LDO could supply is 200mA. While, the customer measured the voltage of 1.3V point, it's value is 2.7V not 1.3V, the output voltage swing of SN65LVDT101 is also incorrect. Then he removed two 50 Ohms termination resistors and detected again, the output of LDO is 1.3, it's correct. He used a Source Voltage to replace LDO, the output voltage swing is also incorrect.
Then he tried another method the Thevenin Termination. This time the output voltage swing is correct.
I know Thevenin Termination is based on standard LVPECL termination, but why standard LVPECL termination couldn't work normal in this application?
Any comments or suggestions are welcome.
Regards,
Ricardo