Part Number: HVDA551-Q1
On the datasheet, there are two particular features listed:
- Data rate up to 1Mbps
- Supports Can Flexible Data-Rate (FD)
Does the latter imply that the transceiver can accept CAN-FD messages with payloads of up to 64 bytes? Or only that the data rate can be adjusted up to 1Mbps, but the payload has to remain at a maximum 8 bytes?
Thanks,
Thomas