Part Number: DP83848K
Hello TI Engineers,
I have a service request which the customer asks the questions below. Can you please provide some answer for the customer?
Customer’s request;
“ I am using DP83848K Ethernet transceiver interface with the MCIMX6U6AVM08AB Processor.
1.Mode selected for my application is MII . The clock for Ethernet transceiver is 25Mhz which can be sourced from Clock or oscillator.
My question is Can this 25MHz to the Ethernet transceiver be sourced from the clock generated in the Processor? Will it work?
2. I hope the Rbias resistor is used to set-up critical bias currents. In my design , I have used an RJ45 connector(J0011D21BNL) with integrated transformer. The recommended resistor and capacitor are used for TPI network
Please clarify how should I calculate power consumption ? How to calculate ICT
3.My design uses external PI and RC filters between the PHY and RJ45 . Is it recommended to have it for filtering ?
Additional question;
In Datasheet the maximum power dissipation is 264mW. The Idd10 current is 92 mA(typical). VDD is 3.3V. The calculated power is 303.6 mW which is exceeding the datasheet limits . How is the maximum power calculated? "
Thank you.
Best regards,