This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/SN65DSI84-Q1: No lock issue

Part Number: SN65DSI84-Q1

Tool/software: Linux

Hi team:

We are using  SN65DSI84-Q1 to convert DSI to LVDS,However, they can't get lock.

The input clock is from their processor Intel X86 and frequency is about 277MHz.

The register dump is as below, you can see E5 is 81.

2、 Initialization Sequence:

3、The schematic is as attached:

Is there anything wrong with our setup? thanks!