Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: DS90UB914A-Q1
[ DS90UB913A-Q1 ] Which is the default mode either 10-bit or 12-bit?
Hi,
Which is the default mode of DS90UB913A-Q1 either 10-bit or 12-bit after power-up?
I know the mode 10-bit or 12-bit of DS90UB913A-Q1 is set by DS90UB914A-Q1 through back-channel. And, from the 0x05 register of DS90UB9i13A-Q1, it seems that both modes are NOT selected. Please help to make sure the default mode just after power-up.

Thanks,
Ken
<Related Post>:
DS90UB914A-Q1: MODE Settling Time
e2e.ti.com/.../2540410