Part Number: DS90LV012A
Other Parts Discussed in Thread: DS90LV011A, , SN64BCT25244
Hello,
I am using DS90LV012ATMF as a clock buffer at 50MHz. I would like to use it to drive a 50R input. Is the driver capable of operating at such load without MTBF degradation? I cannot prove its suitability from the datasheet information, since it does not mention anything regarding drive strength (mentions only sink 100mA).
Best regards,
Lefteris Loghis