Part Number: HD3SS3415
Other Parts Discussed in Thread: HD3SS3412
Hi,
I require HD3SS3415 or HD3SS3412 for the following uses:
1. Able to switch 4 lanes of MIPI signals running at a max bitrate of 1.5Gbps
2. Able to switch LVDS signals with 1.2Gbps
3. In general, I wish to employ it for USB3.0, PCIe, HDMI 2.0a, DP 1.4 switching.
Q1: Can this IC be good for the above tasks?
Q2: The MIPI standard low power mode defined with low rate (~10Mbps) high amplitude (~ 1.2V) switching - will it support this feature?
Q3: Will it be able to switch single-ended signals running @ 1.8V? also in the order of ~ 10Mbps?
Thanks in advance
Oded A