Part Number: TMDS171
Other Parts Discussed in Thread: DS22EV5110
Hi,
The DVI specification 1.0 defines a maximum Interpair skew at receiver of 0.6*Tpixel. This means that the maximum interpair skew is dependant of Tpixel value (system frequency/ video resolution).
In the TMDS171 datasheet is specified a maximum interpair skew (at receiver) of 1.8 ns (page 8 TMDS Differential Input). Following this description the TMDS171 interpair skew tolerance is independent from Tpixel. If true this means that also at low Tpixel frequency this specification must be meets; this is more tight than DVI specification.
Eg: for a Tpixel of 100MHz by DVI specification we have a maximum tolerated interpair skew of 16.667 ns that is around 10 times more tolerant respect to TMDS171 specification.
Anyone can confirm that my understanding is right? Is TMDS171 have less interpair skew tolerance than DVI specification ?
Thank you in advance.