Part Number: TUSB215
Dear Team
For the TUSB215 test in the datasheet, every time should power on(RSTN) to reset the device to have a test, so for a real application, the system will only power up one time and the TUSB215 will be reset. After that, the TUSB215 will always powered up without reset, will this a problem?
Customer mentioned the device need toggle RSTN every time for the test even without change the configuration, so this is because the USB TEST_PACKET or some other things?
the TUSB215 host side application can be used without MCU to control the RSTN, right?
Thanks for your help.
BR.
Jun Shen