This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Selection of synchronous clock mode for single camera

Part Number: DS90UB954-Q1


Hi team,

Our customer will use single camera with 953.

Since there is only one camera, it does not need to be a synchronous clock.

There are advantages of using synchronous clock mode, such as there is no local oscillator, higher BC frequency, but neither of them has big influence in their case.

Is there a functional difference between synchronous mode and asynchronous mode, and there are other performance differences?

Best regards,

Tomoaki Yoshida

  • Yoshida-san,
    As you highlighted there are some advantages with using the synchronous mode, but both are supported and can be used based on their use case.
    For additional information on the clocking modes in the ADAS devices, please refer to the video training modules on the FPD-Link learning center link below.