This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: Do we have some suitable solution can achieve a lot of LVDS input, and then with a serdes to transmit to other side with long line?

Part Number: DS90UB964-Q1


Hi team,

Do we have some device can achieve the function below? Thanks.

we want to use three sensors, every sensor has 1 clock signal, 4 data signal.

  • Frank,
    please use TI's helpme system.
    for your issue, sensor output has 1clock&4data NOT 2Gbps LVDS? if yes, the i/f is DPHY, so the block diagram is not correct. you can use TI's UB935 accompanied with sensor, and then select UB960 in the FPGA side, each sensor should have one cable for transmission.

    best regards,
    Steven