Part Number: DS90UB954-Q1
TI team
Thank you for always support to us.
I understood the DS90UB954-Q1 support dual inputs.
I have three questions.
Our system has two same cameras(means each camera's serializer is the same slave adress.)
1. How can we get to change the output signal from port_0 to port_1 (or from port_1 to port_0) during operation ?
Could you tell us the output signal changing command?
2. If the DS90UB954-Q1 set to dual mode when power on, could the DS90UB954 get the remote access to each camera(DS90UB953 and remote device) on same timing ?
※ If only one camera is connected, will the error be occurred?
3. If the DS90UB954-Q1 set to dual mode after power on, could the DS90UB954 get the remote access to each camera indivdualy?
Thanks and best regards,
Kinugawa.
Sharp corp.