Part Number: TPS2546
HI engineers:
Can I use the TPS2546 to get more than 2A output current in USB 2.0 communication?
Thanks!
TIS: Johnsin tao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2546
HI engineers:
Can I use the TPS2546 to get more than 2A output current in USB 2.0 communication?
Thanks!
TIS: Johnsin tao
Hi Johnsin,
Based on the USB BC1.2 specs, in order to be compliant a device must charge at 5V with a max current of 1.5A. However, some portable devices break this compliance and draw more than 1.5A of current. The TPS2546 recognizes this and is able to supply up to 2.4A of current. The three standard BC1.2 charging modes are dedicated charging port (DCP), standard downstream port (SDP), and charging downstream port (CDP). The divider 1, divider 2, and 1.2V divider mode are the non compliant charging modes that the TPS2546 is able to support.
Let me know if this answers your question or not! If so, please click This resolved my issue