Part Number: DS90UB953-Q1
Hi team,
The customer's requirements is as below:
Input MIPI-->through CML level -->LVDS》 Display screen.
The customer would like to use DS90UB953-Q1+DS90UB928-Q1 to achieve his application.
Because his thinks that the input signal is MIPI signal and the output signal is CML level signal for 953.
And the input signal is ML level signal and the output signal is LVDS signal for 928.
Q1: Is his understanding correct? Would you explain what the input signal and the output signal are for 953 and 928?
Q2. If the customer's understanding is incorrect. Would you recommend a suitable application to achieve the customer's application?