Part Number: DS90LV804
Hello,
We are planning to use the DS90LV804 LVDS buffer/repeater in our system to drive LVDS signals at 250 Mbps (ADC output data lines) through a 3 metre length of Cat6 cable. I’m assuming that since LVDS uses a current-mode driver there is no current dependence on the capacitance of the cable or on capacitance of TVS diodes used at the cable-side of the buffer/repeater? And that we can therefore expect power supply current for 250 Mbps data rate to be as shown in Figure 6 of the datasheet, i.e. < 140 mA?
Best regards,
Peter.