Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD205A: V|AB| or V|YZ|

Part Number: SN65MLVD205A

Hi all

Would you mind if we ask SN65MLVD205A?
On the datasheet P5, there is the description which V|AB| or V|YZ| are min 480mV to max 650mV.
On the test Figure 14. Differential Output Voltage Test Circuit, are A/Y and B/Z's voltage follows?
-A/Y : 0.7V-1.3V(Alternately)
-B/Z : 1.3V-0.7V(Alternately)

Kind regards,

Hirotaka Matsumoto