This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH947-Q1: OLDI Differential Input Voltage

Part Number: DS90UH947-Q1

Hi Team,

If the DS90UH947-Q1 is receiving OLDI signals that are greater than 600mV, what are the resultant potential consequences?

Thank you,

Jared

  • Jared,
    This can affect the performance or functionality of the device. The device is only guaranteed to perform as per specifications when it is within the max value, although this should not damage the device as long as the absolute maximum rating in the datasheet is not exceeded.